This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: CCS_V3.3 Windows10 Pro AMD



Tool/software: Code Composer Studio

Hi,

I was using CCS3.3 in HP laptops(intel i5 processor) with Windows10 Enterprise. I had no problem with that configuration.

Now, I set up the CCS3.3 in Lenovo Laptops (AMD processor) with Windows 10 Pro. I can open the Code Composer Setup and select the board setup. However, Code Composer Studio cannot opened. (CCS opening screen is appered but then it is shut down itself.)

Is there anyone facing this problem and solve it?

Thank you

  • Hello,

    Unfortunately CCSv3.3 is completely unsupported on Windows 10. The behavior is often hit or miss for many. The only recommendations I can provide are to make sure cc_setup.exe and cc_app.exe are configured to run as administrator and in XP SP3 compatibility mode. Otherwise there is not much support I can give.

    Thanks

    ki