Other Parts Discussed in Thread: AWR1843, CC2650
Tool/software: Code Composer Studio
Dear Sirs
I installed Code Composer Studio 9.1.0, and I need Hercules Safety MCUs and mmWave Sensors. After installing and updating CCS I'm importing two projects, one works with AWR1843 and another works with TMS570LC34xx. And in the second project I've got an error:
"This project was created for a device not currently recognized - Cortex R.TMS570LC43xx. Re-run CCS installer on your existing CCS location, ensure the Product Family for your device is selected, and proceed with installation if it wasn't. See 'Help > Check for Updates' to check if support for this device is available through a CCS update. Migrate the project to closest matching supported device by adjusting project properties. Or contact TI for support if using experimental silicon."
I have already tried to re-install CCS, but have same result. If I install Hercules Safety MCUs first, and install mmWave after it, I have the same problem with AWR device. How can I resolve this issue?
Regards, Tovmachenko D.K.