Part Number: TMS320DM8148
Tool/software: Code Composer Studio
Can i able to program my Davinci media processor TMS320DM8148 in CCS IDE?. Or which Platform/IDE will support these processors. Kindly provide some suggestions.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320DM8148
Tool/software: Code Composer Studio
Can i able to program my Davinci media processor TMS320DM8148 in CCS IDE?. Or which Platform/IDE will support these processors. Kindly provide some suggestions.
I mean what OS will you be running the the ARM core that is on DM8148? For example will you be running Linux on it or SYS/BIOS or something else?
John
I include sys/bios installer with my CCS v9.3 in windows.
http://www.ti.com/tool/SPRC265
http://www.ti.com/tool/SPRC264
From the above links i downloaded img and dsp lib files. I am new to this Davinci media processor, kindly provide me the procedure for programming DM8148 using CCS and SYS/BIOS.
I am not sure what development board you have. I can find a few different ones online. Mistral, eInfoChips and another from Z3. None appear to have an onboard debug probe so you would have to use an external JTAG debug probe to connect CCS to the board for programming.
Looking at our webpage for this device it states:
This product does not have ongoing direct design support from TI. For support while working through your design, you may contact one of the following third parties: D3 Engineering, elnfochips, Ittiam Systems, Path Partner Technology, or Z3 Technologies.
To program this board you will need:
I found a Mistral DM8148 EVM in our office. I will see if I can get a program loaded onto it.
Regards,
John
Ok I was able to get my Mistral DM8148 board working.
I have CCSv9.3, Mistral DM8148 EVM, XDS200 class debug probe.
I have the Mistral board powered by a 12V power supply
The XDS200 is connected to the 20pin JTAG header in the middle of the board.
In CCS created a project by going to the project menu and selecting New CCS Project
I entered DM8148 in the filter box on the left. I then selected EVMDM8148 in the device/board drop down.
For the connection I selected Texas Instruments XDS2xx USB Debug Probe
On the Cortex A tab I gave the project a name and selected "Hello World" from the basic examples.
Clicked Finish. I now have a project in my project explorer for the Cortex A8 core on this device.
I click on the build button to build the project. This may take a while as it has to build the C runtime support library the first time.
I click on the bug button to launch the debugger. It clonnects to the A8, initialized the memory, loads my program onto the device.
So I can confirm that CCSv9.3 supports programming DM8148.
Regards,
John
I'm not working with EVM board, we have our own development board with DM8148 media porcessor IC.
When searching regarding this, we came across the dsp image file which has to be load into DM8148 through sd card via sys/bios to start programming .
Kindly help me with this, We are not clear with the exact procedure to be followed.
user4764564 said:I'm not working with EVM board, we have our own development board with DM8148 media porcessor IC.
When searching regarding this, we came across the dsp image file which has to be load into DM8148 through sd card via sys/bios to start programming .
I won't be able to help with that. The original question was regarding loading via CCS. I will loop in someone from the DaVinci team to comment.
Regards,
John
Hi,
The DSPLib and ImageLib you referred to don't support DM8148 device. From the download pages, it clearly indicates which device the library is for. They are for C64x, C66x, C67x, and C55x. None of them is for DM8x.
On the other hand, DM8148 is an old device. We do not have any collateral or resource beyond what you see on the product folder. You may search the E2E forum for archived posts of previous discussions which may help address your questions. For more info on DM8148 support, please see the FAQ in
https://e2e.ti.com/support/processors/f/791/t/813421
Rex