This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/66AK2H14: CrashReportJob and internet connection problem

Part Number: 66AK2H14


Tool/software: Code Composer Studio

Hi!

I use CCS 7.4 with the Ubuntu 16.04. (Also tried 9.4 and 5.5)

And there is the problem with CCS. 

In the progress window appears the process "CrashReportJob" after CCS starting.

 And it doesn't disappear.  Even if I click "cancel operation".

Also in the "App Center" window near the tools loading icons display instead of "select" button.  

And if I start "check for updates" nothing happens. 

But sometimes it reachs 1% after 30 minutes "thinking". The problem can be in internet connection speed, but in browser and terminal everything OK.

Help me please.

Nikolay