Hello everyone,
we are trying to use a DSK C6713 together with CCS v3.3. However CCS v3.3 makes serious troubles.
CCS v3.3 (with or without the Service Release 12 Update) does not start. It shows the splash screen but as soon as the GUI should show it simply terminates. No error message, no hints, it just exits.
The system is running an up to date Windows XP SP3 (32bit). Several tries to fix CCS 3.3 by reinstalling didn't fix the issue. Note that the installation runs through without any complications or messages. Also CCS 3.3 is started by a user with admin rights.
The latest drivers for the DSK C6713 are installed (from http://support.spectrumdigital.com/ccs33/).
Any experiences with this behaviour? What could be wrong?
Best Regards,
Sebastian