Part Number: TDA3LX
Tool/software: Code Composer Studio
I am trying to connect code composer version9 with target ezdsp F28335. unfortunately, the connection test failing with the following errors. Could you please help me with this matter.
-----[Print the board config pathname(s)]------------------------------------
C:\Users\alotaibs\AppData\Local\TEXASI~1\
CCS\ccs930\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 560/2xx-class product.
This utility will load the program 'sd560v2u.out'.
E_RPCENV_IO_ERROR(-6) No connection: DTC_IO_Open::dtc_conf
Download failed for file C:\ti\ccs930\ccs\ccs_base\common\uscif\xds560v2.out
An error occurred while soft opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-250' (0xffffff06).
The title is 'SC_ERR_ECOM_EMUNAME'.
The explanation is:
An attempt to access the debug probe via USCIF ECOM has failed.
[End: Spectrum Digital XDSPRO USB Emulator_0]