This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hello,
I have been using CCS8.0 for a long time but suddenly this error is occuring:
*** Build of configuration Debug for project Example_2805xECap_Capture_Pwm ****
C:\ti\ccsv8\utils\bin\gmake -k all
"C:\\ti\\ccsv8\\utils\\bin\\gmake" -k all
Cannot run program "C:\ti\ccsv8\utils\bin\gmake": The system cannot find the file specified.
Error: Program "C:\ti\ccsv8\utils\bin\gmake" not found in PATH
PATH=[C:\ti\ccsv8\ccs_base\common\bin;C:\ti\ccsv8\ccs_base\common\uscif;C:\windows;C:\Program Files (x86)\Intel\iCLS Client\;C:\Program Files\Intel\iCLS Client\;C:\windows\system32;C:\windows;C:\windows\System32\Wbem;C:\windows\System32\WindowsPowerShell\v1.0\;C:\Program Files (x86)\Intel\Intel(R) Management Engine Components\DAL;C:\Program Files\Intel\Intel(R) Management Engine Components\DAL;C:\Program Files (x86)\Intel\Intel(R) Management Engine Components\IPT;C:\Program Files\Intel\Intel(R) Management Engine Components\IPT;C:\MATLAB7\bin\win32;C:\Program Files\MATLAB\R2018b\bin;C:\Program Files\MATLAB\R2018_A\bin;C:\Users\KARTHIK R\AppData\Local\Microsoft\WindowsApps;;C:\MentorGraphics\PADSVX.2.4\SDD_HOME\CAMCAD]
Error: Program "C:/ti/ccsv8/utils/bin/gmake" is not found in PATH
Though i have checked the path and this file is present there. I have also followed the steps like:
1. disabling the antivirus, allow permission to ccstudio in firewall and then installing.
2. Reinstalling with new workspace.
anybody can provide the solution to this?
Hello,
Avichal Srivastava said:1. disabling the antivirus, allow permission to ccstudio in firewall and then installing.
Antivirus and related security software is usually the main cause of this error. Disabling such software usually resolve the issue. Your case must be a different issue.
Can you check the permissions of the gmake executable? Can you run it manually without issue?
If so, can you temporarily modifying the system PATH so that only the directories related to CCS are in there? You can open a new console and set the PATH that way, and then browse to the ccs executable (ccsv8\eclipse\ccstudio.exe) and run it.
Thanks
ki
Hello Ki,
Can you check the permissions of the gmake executable- i have checked and the permissions are ok.
Can you run it manually without issue?-I tried by double clicking the gmake.exe file and there was no error message popped up.
If so, can you temporarily modifying the system PATH so that only the directories related to CCS are in there?- I am unable to find the setting in the software for this, could you please give the steps.
Regards
Avichal Srivastava said:If so, can you temporarily modifying the system PATH so that only the directories related to CCS are in there?- I am unable to find the setting in the software for this, could you please give the steps.
If you echo the PATH in the command prompt, there usually is a lot of stuff in the PATH:
hence use the "set" command to set the PATH to only have paths needed by CCS to run.
> set PATH=[path];[path]; etc
just keep that paths that point to things related to CCS. Since paths can vary depending on the user's environment, you will need to figure out what paths are needed.
after setting the path, launch CCS manually by running <CCS8 INSTALL DIR>\ccsv8\ccs\eclipse\ccstudio.exe from the same command prompt
Please provide the project metadata files. Those files would be the three .*project files in the project folder. Zip them up and attached the zip to this thread.
Thanks
ki
Thanks. Your project metadata looks fine. I can build the project without issue.
When I carefully check your last screenshot again, I noticed something odd in the PATH. The directory before c:\ti\ccsv8\utils\bin does have a semicolon separator at the end. It looks like a whitespace. There should be a semicolon like the other directories (except for the last directory in the path). Can you carefully check your PATH again?
Thanks
ki
Hello ki,
I have noticed one thing that when i am installing the ccs in my system, everytime there is a firewall permission window pop up for tidcs(though have allowed in the firewall settings) which previously never occurred and using the same installation file in other systems, this firewall permission is not coming and there is no error in build as well.
Regards,
Avichal
Is your username "KARTHIK R"? If so, the whitespace character can cause an issue. Please see:
https://e2e.ti.com/support/tools/ccs/f/81/t/740719?tisearch=e2e-sitesearch&keymatch=faq%3Atrue
Can you try with a user account that does not have any spaces in the username?
Thanks
ki