This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TI C/C++ Compiler
my workstation is offline, so i can only download compiler from ti website and install it locally, the version i downloaded is c2000 18.1.7 LTS windows installer, and the compiler is installed at ti/ccsv6/tools/compiler/, in the directory there exists other old versions of compiler and they are out dated.
here comes the thing, when i start a new ccs project, only old version compilers can be selected, the newly installed one doesn't show up, and i checked the preference contents, the ccs composer studio/compiler still shows old version, and i add the installation path and press fresh btn, nothing occures.
so how can i fix this?
user4734970 said:here comes the thing, when i start a new ccs project, only old version compilers can be selected, the newly installed one doesn't show up, and i checked the preference contents, the ccs composer studio/compiler still shows old version, and i add the installation path and press fresh btn, nothing occures.
The new compiler should get detected when the refresh button is pressed.
Can you take a screenshot of your compiler discovery preferences? Something like the below:
In my screenshot above, I added the path to c2000 19.6.0.STS and then pressed the Refresh button to have it detected by CCS.
Thanks
ki
Hi,
Just adding to Ki's reply above, I am unsure what may be happening in your case. I just downloaded the compiler and installed under the same directory in my CCSv6.2.0 install here.
I can attest it is properly acknowledged by the IDE.
I see you already clicked on the "Refresh" button, which should trigger the acknowledgment. Could try restarting CCS instead? This should trigger a re-scan of the compilers and get it added to the tool.
Hope this helps,
Rafael
hi,Rafael
it is not convinent to take screen shots, that pc not allowed to access the internet,and taking photo also forbiddened.
I followed exact steps Ki ang you did, but it didn't work, I am wondering something must be wrong for the strategies used by my administrator on that pc, I tried those steps on my own pc, it works well.
thanks for your help.