Part Number: AFE4490SPO2EVM
Other Parts Discussed in Thread: MSP430F5529, MSP-FET
Tool/software: Code Composer Studio
Is there anyway to program/debug the AFE4490SPO2EVM board through Code Composer Studio (CCS)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AFE4490SPO2EVM
Other Parts Discussed in Thread: MSP430F5529, MSP-FET
Tool/software: Code Composer Studio
Is there anyway to program/debug the AFE4490SPO2EVM board through Code Composer Studio (CCS)?
The AFE4490SPO2EVM has J1 which is a 6-pin "eZ430 RF Header" to which a debugger could be connected to program or debug the on-board MSP430F5529 with CCS, but J1 is not installed by default.
To just program the board, SW2 is used to enable boot strap loader (BSL) MSP430 firmware, which can be used to program the MSP430F5529 via the USB connector J4.
Hi Farzad,
If you need to debug/modify the firmware of AFE4490EVM, you would need following JTAG connector along with the MSP-FET debugger. This JTAG connector can be plugged into J3 of AFE4490EVM for debugging as well as programming using CCS.
https://www.digikey.in/product-detail/en/tag-connect-llc/TC2050-IDC-NL/TC2050-IDC-NL-ND/2605367.
Regards,
Prabin.
That TC2050-IDC-NL doesn't have the retaining fingers, and has a 10 pin IDC socket which won't plug in directly to a MSP-FET.Prabin Yadav said:This JTAG connector can be plugged into J3 of AFE4490EVM for debugging as well as programming using CCS.https://www.digikey.in/product-detail/en/tag-connect-llc/TC2050-IDC-NL/TC2050-IDC-NL-ND/2605367.
The TC2050-IDC-430 looks to the better cable to use since:
I haven't tried the TC2050-IDC-430 myself, but just checked the manufacturers drawing https://www.tag-connect.com/wp-content/uploads/bsk-pdf-manager/TC2050-IDC-430_Datasheet_10.pdf
Hi Parbin,
I'm doing it the same way. Using the JTAG connector cable, I interfaced the MSP-FET with the AFE4490EVM.
The board is powered through the MSP-FET, the LED on the EVM is dim.
When I try to debug the MSP430 using CCS, I get this error:
Error connecting to the target: Unknown device
OS: Windos 10
CCS v9.3
Hi Farzad,
I suggest you to measure the supply voltage of MSP430. You can probe the voltage node called MSP_DVCC and it should be ~3V.
Did you try using the CCS with EVM plugged to PC? if not, can you please give it a try.
Just to make sure that the MSP430 is still functional you can try to load the compiled file using bootloader as described in section 6 of AFE4490EVM's user guide.
Regards,
Prabin.
Hi Prabin,
Thanks.
Updating the firmware using the method that is described in Sec. 6 of user guide does not work. Actually, the button 'Upgrade Firmware' stays disable.
I'll check voltage of MSP_DVCC and and get back to you soon.