Tool/software: TI C/C++ Compiler
Hi,
I used to be able to find these files at but this link no longer works, and I suppose is out of date anyway since we're up to CCS10. Is there somewhere else where I can find these files.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In the CCS directory below, you can find the header files and linkers.
C:\ti\ccs1000\ccs\ccs_base\msp430\include
targetdb files are found below.
C:\ti\ccs1000\ccs\ccs_base\common\targetdb
Hello,
Sorry for the delay. I am still looking into these plat form specific files and hope to have some feedback next week.
Hi,
I have been able to put this off until now by working on other projects, but I can't delay any longer. Even if you're able to just tar/zip up the `common` and `msp430` directories and post them here or email them to me that would do for now.
Thanks.
Parakleta,
The directories are quite large to attach here on e2e. The easiest way is to download and install CCS. You can download it below.
http://software-dl.ti.com/ccs/esd/documents/ccs_downloads.html
I have also included the directories at the box link below if you do not want to install CCS.
Thanks for the box link, that will get me started. There was some irrelevant files but they don't matter, but it appears the `msp430/lib` directory is missing with support libraries. I'm not using any of the MCUs supported by that directory currently, but will be in a future project.
I disagree that downloading CCS is the easiest (although I suppose it being the only way makes it the easiest by default). Downloading nearly 1GiB of data just to extract (what was previously) a 7MiB package in support of a 24MiB compile tool seems wasteful.
The previous files that I was able to access were called `ti_msp430pack_header_files_setup64_8.2.0.bin` and `ti_msp430pack_header_files_setup64_9.1.0.bin` if that makes it easier for you to figure out how to find/make them again.