Part Number: ADS8361
Tool/software: Code Composer Studio
Hello,
I'm having issues interfacing the ADS8361 chip with the DSK6713 through the McBSP on that board. I'm following the SLAA164 application note and trying to run this code on CCS 5.5.0. I'm able to get the DSP board to accept one value from the ADC, but after the first value, the RFULL bit of the Serial Port Control Register is raised. This prevents the read interrupt from triggering, and I can't read in any values after the first.
I've been modifying the McBSP configuration, trying difference sampling rates, frame lengths, frame periods, and even at very low rates (~2 ksps), the board still overflows. I've checked that the RRDY bit in the SPCR reads 0 when my interrupt routine closes, so I'm very confused how the receive buffer is overflowing.
If anyone has experience interfacing these two components, let me know if there's something I'm missing that could cause this error.
Thanks!