This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Is there any way to convert the intel hex file to a binary file or directly generating a binary file from code composer v9 as its not from the option , to burn the .bin file using boot loader and LM flash programmer?
Thanks for your fast reply ,
i checked the thread and used this command as it is "${CCS_INSTALL_ROOT}/utils/tiobj2bin/tiobj2bin""${BuildArtifactFileName}""${BuildArtifactFileBaseName}.bin""${CG_TOOL_ROOT}/bin/armofd""${CG_TOOL_ROOT}/bin/armhex""${CCS_INSTALL_ROOT}/utils/tiobj2bin/mkhex4bin"
in the Post-build steps section inside the build options then rebuild the project but the .bin file wasnt generated is there something missing in this command?
Hi,
The command looks ok, but can you see if the Console output shows a specific error?
If it is successful, the tail of the build should be something similar to the output below (copied from the blinky Tivaware example):
Console said:Building target: "blinky.out"
Invoking: ARM Linker
"C:/CCSv10_0_0/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me -O2 --define=ccs="ccs" --define=PART_TM4C129XNCZAD --define=TARGET_IS_TM4C129_RA0 -g --gcc --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --ual -z -m"blinky_ccs.map" --heap_size=0 --stack_size=512 -i"C:/CCSv10_0_0/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/lib" -i"C:/CCSv10_0_0/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/include" --reread_libs --diag_wrap=off --display_error_number --warn_sections --xml_link_info="blinky_linkInfo.xml" --rom_model -o "blinky.out" "./blinky.obj" "./startup_ccs.obj" "../blinky_ccs.cmd" -l"C:/ti/TivaWare_C_Series-2.2.0.295/driverlib/ccs/Debug/driverlib.lib" -llibc.a
<Linking>
Finished building target: "blinky.out"
"C:/CCSv10_0_0/ccs/utils/tiobj2bin/tiobj2bin" "blinky.out" "blinky.bin" "C:/CCSv10_0_0/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/bin/armofd" "C:/CCSv10_0_0/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/bin/armhex" "C:/CCSv10_0_0/ccs/utils/tiobj2bin/mkhex4bin"**** Build Finished ****
I am not sure if it was an artifact of the copy/paste on your post, but the command line does not have any spaces between the different parameters. It should be something like this:
Console said:"${CCS_INSTALL_ROOT}/utils/tiobj2bin/tiobj2bin" "${BuildArtifactFileName}" "${BuildArtifactFileBaseName}.bin" "${CG_TOOL_ROOT}/bin/armofd" "${CG_TOOL_ROOT}/bin/armhex" "${CCS_INSTALL_ROOT}/utils/tiobj2bin/mkhex4bin"
Regards,
Rafael