Part Number: TM4C1294NCPDT
Other Parts Discussed in Thread: EK-TM4C1294XL
Tool/software: Code Composer Studio
In tiware directory there is sample of program called blinky. I build this program using composer studio but how I can build binary which can be programed in on chip flash which I can run after reset or power cycle.
I tool blinky.bin file and with lm flash programmer programmed blinky.bin starting at address 0x4000 , but I cannot see it running and blinding LED.
What are the steps to build so it will run programmed at address 0x4000.
Thaks