Part Number: TMS320DM642
Tool/software: Code Composer Studio
When trying to load software to the target or debug software on the target, CCS outputs the following error message:
C64x: File Loader: Verification failed: Values at address 0x80000000 do not match Please verify target memory and memory map. C64x: GEL: File: C:\project\example.out: a data verification error occurred, file load failed.
The development PC has Windows 10 installed.The CCS version is Version: 7.3.0.00019. The TI processor is TMS320DM642. Initially the debugger was working on Windows 10. The last time working with this debugger was one or two months ago. The software was not modified.
Does anyone can give support for this problem?
Thanks in advance.