Part Number: CCSTUDIO
Tool/software: TI C/C++ Compiler
Problem with PRAGMA and undefined symbols after messing with syntax highlighting and scalability options.
I'm using the C2000 Compiler Ti v18.1.4.LTS but I don't think the issue is compiler specific.
I have a large file and somehow during my attemps to get syntax highlighting working in the editor I set the compiler option --cpp_default.
This caused many compiler errors and I could not find a checkbox in the project properties to undo this option so finally had to
edit the compiler flags directly and remove the --cpp_default option to get the project to build.
I believe you can set the compiler flags for each file and somehow that one large file had option --cpp_default set which
caused the issue.
I spent some time in the project properties trying to resolve the issue with the C Dialect and C++ Dialect drop down boxes but that didn't do what I wanted.
The problem is resolved but I thought I would post this in case anyone else had this same issue.