Other Parts Discussed in Thread: ENERGYTRACE
Tool/software: Code Composer Studio
Hello everyone,
first post here.
I have a Launchpad board with MSP432P401R, red, v2.0.
Running latest CCS locally (Version: 10.1.0.00010) with latest SDK (3_40_01_02).
I'm trying to follow this EnergyTrace example:
dev.ti.com/.../node
Problem is, I'm not able to complete "Task 6":
dev.ti.com/.../msp432_03_low_power_modes.html
It says to stop debugger, disconnect the board, remove all jumpers less "3V3" and "GND", reconnect the board.
Then to click on the "Energy Trace" button in the CCS main toolbar.
But nothing happens, except for a brief "Detecting Energy Trace Pod ... XCD110.xml", or something like that
No energy measurement is taken, do I don't get the expected output (the figure after "we see a new, more accurate, result for our current consumption as shown below")
I just can't figure out what to do.
Any hint?
Thanks!
Fernando