Part Number: AWR1843
Tool/software: TI C/C++ Compiler
Hello All,
I am using the MCAL GPT module with SYS/BIOS. In my application i need to use the timers configured by the GPT module with the Sys/Bios , so for the timer to work i thought i should link the ISR of the Gpt timer with the OS vector table for the ISR to Come.
I configured a Hwi instance in the OS configurator with an ISR name as that used by the Gpt timer. How can i configure a HWI instance, do i need to configure a timer in the OS configurator as well or not?
How can i solve this error?
SYS/BIOS version 6_73_01_01.
the *.cfg file: 8875.mss_mmw.cfg
Thank you
Nada