This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I created project in CCS4. i have .C and .H file. i always used these 2 files in project. but TI- gang programmer needs .int, .hex, .a43 file format.
can anybody tell me how to deal with this. I got .out file when i build the program. please tell me how to created .hex file out of .out file.
Just to add to Ki's reply, this task has been simplified for MSP430 projects. If you go to Project Properties->C/C++ Build->Build Steps tab, under "Apply Predefined Step", there are a couple of predefined commands for generating TI-TXT and Intel hex outputs. If you select one of the them, the post build command will be populated with the appropriate command and will always run as a post-build step on your .out file when you build your CCS project. You can easily customize the command to add other options or output a different hex format.
Yes it is a command line executable. You can open a DOS command window, browse to the location of the hex<isa>.exe and run 'hex<isa>.exe -h' to get more documentation.
ex to run the help (for ARM):
> cd C:\Program Files\Texas Instruments\ccsv4\tools\compiler\tms470
> hex470 -h
And if you are using MSP430, I suggest you use the post-build step as Aarti suggested.
Isn't .a43 the same as Intex hex format? Or were you expecting a different hex format? If it is the same as Intel hex, you can choose the Predefined post-build step in CCS as noted in the previous post in this thread, and change the -o (output file) option to .a43 extension. If you are looking for a different hex format, please check Chapter 11 of the MSP430 Assembly Language Tools Users Guide for the formats supported by the hex converter.
FYI
I followed the steps above with CCSv4.2.4 and selected "Create flash image: Intel-HEX" and got the error below.
"C:/Program Files/Texas Instruments/ccsv4/tools/compiler/C6000 Code Generation Tools 7.2.6/bin/hex6x.exe" -i "M2_EVM6472.out" -o "M2_EVM6472.hex" -order MS -romwidth 16
error: bad argument to option -order: should be one of {M,L}
gmake[1]: [post-build] Error 1 (ignored)
' '
Build complete for project M2_EVM6472
hi I want to convert my .out file to .hex format. I have run -i <my file path>test.out command and I have got
translating d:......\test.out to to Intel format....
"D:\......\test.out" ==>vecs
"D:\......\test.out" ==>.test
"D:\......\test.out" ==> .cinit
but my .hex file is not getting generated.
is i have to run any other commands along with that ?
Hi
I have written a code and now I want to generate its hex file and want to port it to hardware without using flash burn. But I can't find any thing like 'hex utlity' or "flash burn utility" in my CCSv5.5.
What is the reason?
Thankyou
Maheen