This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I created project in CCS4. i have .C and .H file. i always used these 2 files in project. but TI- gang programmer needs .int, .hex, .a43 file format.
can anybody tell me how to deal with this. I got .out file when i build the program. please tell me how to created .hex file out of .out file.
CCSv4 comes with a utility to convert your out file to hex.
<INSTALL DIR>\ccsv4\tools\compiler\<ISA>\bin\hex<ISA>.exe
call it with the -h option for the help.
Thanks
ki
Just to add to Ki's reply, this task has been simplified for MSP430 projects. If you go to Project Properties->C/C++ Build->Build Steps tab, under "Apply Predefined Step", there are a couple of predefined commands for generating TI-TXT and Intel hex outputs. If you select one of the them, the post build command will be populated with the appropriate command and will always run as a post-build step on your .out file when you build your CCS project. You can easily customize the command to add other options or output a different hex format.
Yes it is a command line executable. You can open a DOS command window, browse to the location of the hex<isa>.exe and run 'hex<isa>.exe -h' to get more documentation.
ex to run the help (for ARM):
> cd C:\Program Files\Texas Instruments\ccsv4\tools\compiler\tms470
> hex470 -h
Isn't .a43 the same as Intex hex format? Or were you expecting a different hex format? If it is the same as Intel hex, you can choose the Predefined post-build step in CCS as noted in the previous post in this thread, and change the -o (output file) option to .a43 extension. If you are looking for a different hex format, please check Chapter 11 of the MSP430 Assembly Language Tools Users Guide for the formats supported by the hex converter.
FYI
I followed the steps above with CCSv4.2.4 and selected "Create flash image: Intel-HEX" and got the error below.
"C:/Program Files/Texas Instruments/ccsv4/tools/compiler/C6000 Code Generation Tools 7.2.6/bin/hex6x.exe" -i "M2_EVM6472.out" -o "M2_EVM6472.hex" -order MS -romwidth 16
error: bad argument to option -order: should be one of {M,L}
gmake[1]: [post-build] Error 1 (ignored)
' '
Build complete for project M2_EVM6472
hi I want to convert my .out file to .hex format. I have run -i <my file path>test.out command and I have got
translating d:......\test.out to to Intel format....
"D:\......\test.out" ==>vecs
"D:\......\test.out" ==>.test
"D:\......\test.out" ==> .cinit
but my .hex file is not getting generated.
is i have to run any other commands along with that ?
Hi
I have written a code and now I want to generate its hex file and want to port it to hardware without using flash burn. But I can't find any thing like 'hex utlity' or "flash burn utility" in my CCSv5.5.
What is the reason?
Thankyou
Maheen