Part Number: TMS320C6713B
Other Parts Discussed in Thread: CCSTUDIO
Tool/software: Code Composer Studio
Hello to all,
I hope someone could help me to solve some troubles I am facing when I try to build my project.
When I do "Build all" in the project, in the linking part I get 10 warnings and the *.obj file is not generated. Also, when linking part is executed I get an exception of win32.
I thank you in advance.
The linking warnings are the next ones:
[Linking...] "C:\CCStudio_v3.1\C6000\cgtools\bin\cl6x" -@"Debug.lkf"
<Linking>
>> warning: creating output section .text:_c_int00 without SECTIONS
specification
>> warning: creating output section .text:_exit without SECTIONS specification
>> warning: creating output section .text:_atexit without SECTIONS specification
>> warning: creating output section .text:_abort without SECTIONS specification
>> warning: creating output section .text:__nop without SECTIONS specification
>> warning: creating output section .text:__register_lock without SECTIONS
specification
>> warning: creating output section .text:__register_unlock without SECTIONS
specification
>> warning: creating output section .text:__args_main without SECTIONS
specification
>> warning: creating output section .text:__auto_init without SECTIONS
specification
>> warning: creating output section .text:_memcpy without SECTIONS specification
Build Complete,
0 Errors, 10 Warnings, 0 Remarks
The exception I get is the next one:
"An unhandled win32 exception occurred in lnk6x.exe[952]"
The Content of the vector files and .cmd file are the next:
lnk6713.cmd file:
-c
-heap 0x400
-stack 0x400 /* very large stack for DSP programs.*/
-rts6700.lib /* floating point library */
MEMORY
{
vecs: origin = 00000000h len = 00000200h
IRAM: origin = 00000200h len = 0003FE00h
SDRAM: origin = 80000000h len = 01000000h
}
SECTIONS
{
"vectors" > vecs
.cinit > IRAM
.text > IRAM
.stack > IRAM
.bss > IRAM
.const > IRAM
.data > IRAM
.far > IRAM
.switch > IRAM
.sysmem > IRAM
.tables > IRAM
.cio > IRAM
"_exit" > IRAM
"CE0" > SDRAM
}
vectors.asm file:
.ref _c_int00
.ref _Codec_ISR
.sect "vectors"
RESET_RST:
MVKL .S2 _c_int00, B0
MVKH .S2 _c_int00, B0
B .S2 B0
NOP
NOP
NOP
NOP
NOP
NMI_RST:
NOP
NOP
NOP
NOP
NOP
NOP
NOP
NOP
RESV1:
NOP
NOP
NOP
NOP
NOP
NOP
NOP
NOP
RESV2:
NOP
NOP
NOP
NOP
NOP
NOP
NOP
NOP
INT4: NOP
NOP
NOP
NOP
NOP
NOP
NOP
NOP
INT5: NOP
NOP
NOP
NOP
NOP
NOP
NOP
NOP
INT6: NOP
NOP
NOP
NOP
NOP
NOP
NOP
NOP
INT7: NOP
NOP
NOP
NOP
NOP
NOP
NOP
NOP
INT8: NOP
NOP
NOP
NOP
NOP
NOP
NOP
NOP
INT9: NOP
NOP
NOP
NOP
NOP
NOP
NOP
NOP
INT10: NOP
NOP
NOP
NOP
NOP
NOP
NOP
NOP
INT11: NOP
NOP
NOP
NOP
NOP
NOP
NOP
NOP
INT12: b _Codec_ISR
NOP
NOP
NOP
NOP
NOP
NOP
NOP
INT13: NOP
NOP
NOP
NOP
NOP
NOP
NOP
NOP
INT14: NOP
NOP
NOP
NOP
NOP
NOP
NOP
NOP
INT15: NOP
NOP
NOP
NOP
NOP
NOP
NOP
NOP
vectors_EDMA file:
.ref _c_int00
.ref _EDMA_ISR
.sect "vectors"
RESET_RST:
MVKL .S2 _c_int00, B0
MVKH .S2 _c_int00, B0
B .S2 B0
NOP
NOP
NOP
NOP
NOP
NMI_RST:
NOP
NOP
NOP
NOP
NOP
NOP
NOP
NOP
RESV1:
NOP
NOP
NOP
NOP
NOP
NOP
NOP
NOP
RESV2:
NOP
NOP
NOP
NOP
NOP
NOP
NOP
NOP
INT4: NOP
NOP
NOP
NOP
NOP
NOP
NOP
NOP
INT5: NOP
NOP
NOP
NOP
NOP
NOP
NOP
NOP
INT6: NOP
NOP
NOP
NOP
NOP
NOP
NOP
NOP
INT7: NOP
NOP
NOP
NOP
NOP
NOP
NOP
NOP
INT8: b _EDMA_ISR
NOP
NOP
NOP
NOP
NOP
NOP
NOP
INT9: NOP
NOP
NOP
NOP
NOP
NOP
NOP
NOP
INT10: NOP
NOP
NOP
NOP
NOP
NOP
NOP
NOP
INT11: NOP
NOP
NOP
NOP
NOP
NOP
NOP
NOP
INT12: NOP
NOP
NOP
NOP
NOP
NOP
NOP
NOP
INT13: NOP
NOP
NOP
NOP
NOP
NOP
NOP
NOP
INT14: NOP
NOP
NOP
NOP
NOP
NOP
NOP
NOP
INT15: NOP
NOP
NOP
NOP
NOP
NOP
NOP
NOP