Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CCSTUDIO: CCSv10 MacOS Sierra - MacBook Pro

Part Number: CCSTUDIO
Other Parts Discussed in Thread: ENERGIA

Tool/software: Code Composer Studio

The error message " The specified directory does not resemble an Energia install. Please select the directory containing the 'energia' executable." is shown when attempting to register the Energia App for a new Energia Sketch in CCSv10 on a MacOS install. The problem does not occur on the Windows install. Using the Java subfolder containing the /hardware folder in lieu of the App does not work either.

  • Bevan,

    CCS does not recognize the Energia install due to a bug in Energia on macOS.  I saw this in Energia 21.  I am not sure what version you are using but there is a workaround.

    Go to the location where you have Energia installed and go to:

    /Applications/.../Energia.app/Contents/Java/lib/

    Open version.txt 

    It likely contains the string "${version}"

    Replace that with "1.8.7E21" or change the 21 to the version of Energia you are using. 

    CCS should now be able to discover Energia.

    Regards,

    John