This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CCSTUDIO: not found in PATH

Part Number: CCSTUDIO

Tool/software: Code Composer Studio

I recently upgraded from CCS 9.10 to 10.10.  I have a Configuration called Lint where I run a batch file to lint my program.  I can run it in CCS 9.10 but in CCS 10.10 I received the following - Error: Program "Z:/ble_cmn/05_Design/Firmware/source/_lint/run_lint_bim.bat" is not found in PATH.  Here's the output:

**** Build of configuration Lint for project cc26x2r1lp_bim_offchip ****

Z:\ble_cmn\05_Design\Firmware\source\_lint\run_lint_bim.bat H:/ccs_workspace/workspace_v10/cc26x2r1lp_bim_offchip Z:/ble_cmn/05_Design/Firmware/source/sdk/4_20_00_35 Z:/ble_cmn/05_Design/Firmware/source/_tools/compiler/ti-cgt-arm_20.2.1.LTS

"Z:\\ble_cmn\\05_Design\\Firmware\\source\\_lint\\run_lint_bim.bat" H:/ccs_workspace/workspace_v10/cc26x2r1lp_bim_offchip Z:/ble_cmn/05_Design/Firmware/source/sdk/4_20_00_35 Z:/ble_cmn/05_Design/Firmware/source/_tools/compiler/ti-cgt-arm_20.2.1.LTS
Cannot run program "Z:\ble_cmn\05_Design\Firmware\source\_lint\run_lint_bim.bat": Launching failed

Error: Program "Z:\ble_cmn\05_Design\Firmware\source\_lint\run_lint_bim.bat" not found in PATH
PATH=[C:\ti\ccs1010\ccs\ccs_base\common\bin;C:\ti\ccs1010\ccs\ccs_base\common\uscif;Z:\ble_cmn\05_Design\Firmware\source\_lint;C:\Program Files (x86)\IBM\RationalSDLC\common;C:\Oracle\odac\app\rosemount\product\11.2.0\client_1;C:\Oracle\odac\app\rosemount\product\11.2.0\client_1\bin;C:\Oracle\app\client\rosemount\product\12.2.0\client_1\bin;C:\Oracle\app\rosemount\product\12.2.0\client_1\bin;C:\app\client\rosemount\product\12.2.0\client_1\bin;C:\windows\system32;C:\windows;C:\windows\System32\Wbem;C:\windows\System32\WindowsPowerShell\v1.0\;C:\windows\System32\OpenSSH\;C:\Program Files (x86)\IBM\RationalSDLC\ClearCase\bin;C:\Program Files (x86)\IBM\gsk8\lib;C:\Program Files (x86)\IBM\gsk8\bin;C:\Program Files (x86)\IBM\RationalSDLC\clearcase\RemoteClient\cteapis;C:\Users\dkelsch\AppData\Local\Microsoft\WindowsApps]

Error: Program "Z:/ble_cmn/05_Design/Firmware/source/_lint/run_lint_bim.bat" is not found in PATH

PATH=[C:\ti\ccs1010\ccs\ccs_base\common\bin;C:\ti\ccs1010\ccs\ccs_base\common\uscif;Z:\ble_cmn\05_Design\Firmware\source\_lint;C:\Program Files (x86)\IBM\RationalSDLC\common;C:\Oracle\odac\app\rosemount\product\11.2.0\client_1;C:\Oracle\odac\app\rosemount\product\11.2.0\client_1\bin;C:\Oracle\app\client\rosemount\product\12.2.0\client_1\bin;C:\Oracle\app\rosemount\product\12.2.0\client_1\bin;C:\app\client\rosemount\product\12.2.0\client_1\bin;C:\windows\system32;C:\windows;C:\windows\System32\Wbem;C:\windows\System32\WindowsPowerShell\v1.0\;C:\windows\System32\OpenSSH\;C:\Program Files (x86)\IBM\RationalSDLC\ClearCase\bin;C:\Program Files (x86)\IBM\gsk8\lib;C:\Program Files (x86)\IBM\gsk8\bin;C:\Program Files (x86)\IBM\RationalSDLC\clearcase\RemoteClient\cteapis;C:\Users\dkelsch\AppData\Local\Microsoft\WindowsApps;]

**** Build Finished ****

I can run the batch file from the command window but not CCS.  Any suggestions?