This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP432P401R
Tool/software: Code Composer Studio
Hi,
I'm using CCS Version: 10.1.0.00010, and am porting code that last ran under v6.3 years ago (time and money stuff)
I'm getting the error unresolved symbol for __delay_cycles, so I'm guessing a flag somewhere, but I don't know where.
I looked in this forum, using __delay_cycles as the keyword but my CCS properties page looks different from the related question answered a year ago.
Any help?
bob s
Hi Bob,
Where is the error coming from? The compiler? Or is it coming from the IDE?
Please provide all the build output from the build console. You can copy and paste to a text file and attach the text file to this thread.
Thanks
ki
Hi,
More information, when I built a project from "new" rather than import an old, and then copied in the very same files, the problem did not appear.
Here's the error build below:
**** Build of configuration Debug__TI_bad for project RapidEnergyUnit ****
/Applications/ti/ccs1010/ccs/utils/bin/gmake -k all
Building target: "RapidEnergyUnit.out"
Invoking: MSP432 Linker
"/Applications/ti/ccs1010/ccs/tools/compiler/ti-cgt-arm_20.2.1.LTS/bin/armcl" -me --advice:power=all -g --display_error_number --diag_wrap=off --diag_warning=225 -z -m"RapidEnergyUnit.map" -i"/Applications/ti/ccs1010/ccs/ccs_base/arm/include" -i"/Applications/ti/ccs1010/ccs/tools/compiler/ti-cgt-arm_20.2.1.LTS/lib" -i"/Applications/ti/ccs1010/ccs/tools/compiler/ti-cgt-arm_20.2.1.LTS/include" --reread_libs --display_error_number --warn_sections --diag_wrap=off --xml_link_info="RapidEnergyUnit_linkInfo.xml" --rom_model -o "RapidEnergyUnit.out" "./EU_board_regmap_v1.obj" "./RTC_Library.obj" "./bfix.obj" "./charge_control.obj" "./dev_config.obj" "./dictionary.obj" "./myList.obj" "./myQueue.obj" "./processNVM.obj" "./processRTC.obj" "./reuc_main.obj" "./reucmds.obj" "./startup_msp432p401r_gcc.obj" "./strncasecmp.obj" "./strptime.obj" "./system_msp432p401r.obj" "./tasking.obj" "./utilities.obj" "../linker_directives.cmd" "/Applications/ti/simplelink_msp432p4_sdk_3_40_01_02/source/ti/devices/msp432p4xx/driverlib/ccs/msp432p4xx_driverlib.lib" -llibc.a
<Linking>
warning #10210-D: creating ".stack" section with default size of 0x800; use the -stack option to change the default size
warning #10210-D: creating ".sysmem" section with default size of 0x800; use the -heap option to change the default size
"../linker_directives.cmd", line 67: error #10099-D: program will not fit into available memory, or the section contains a call site that requires a trampoline that can't be generated for this section. placement with alignment fails for section ".text" size 0x19289. Available memory ranges:
MAIN size: 0x40000 unused: 0x18cdc max hole: 0x18cdc
undefined first referenced
symbol in file
--------- ----------------
__delay_cycles ./reuc_main.obj
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "RapidEnergyUnit.out" not built
remark #10371-D: (ULP 1.1) Detected no uses of low power mode state changing instructions
>> Compilation failure
makefile:156: recipe for target 'RapidEnergyUnit.out' failed
gmake: *** [RapidEnergyUnit.out] Error 1
gmake: Target 'all' not remade because of errors.
**** Build Finished ****
Regarding:
robert schaefer said:"../linker_directives.cmd", line 67: error #10099-D: program will not fit into available memory, or the section contains a call site that requires a trampoline that can't be generated for this section. placement with alignment fails for section ".text" size 0x19289. Available memory ranges:
MAIN size: 0x40000 unused: 0x18cdc max hole: 0x18cdc
Please see: https://processors.wiki.ti.com/index.php/Compiler/diagnostic_messages/10099
As for:
robert schaefer said:undefined first referenced
symbol in file
--------- ----------------
__delay_cycles ./reuc_main.obj
error #10234-D: unresolved symbols remain
I'm not sure why you are getting that error. I'll need to follow up with a compiler expert
Thanks
ki
Regarding ...
robert schaefer said:undefined first referenced
symbol in file
--------- ----------------
__delay_cycles ./reuc_main.obj
I don't know why this happened. But some compiler options that are required when building for MSP432 are missing. They are ...
-mv7M4
--code_state=16
--float_support=FPv4SPD16
Add those options. Then rebuild the entire project.
Thanks and regards,
-George
Keith Barkley said:I think _delay_cycles() only has 1 underscore at the beginning.
Sorry, Keith, but this is a rare occasion where you are incorrect. This intrinsic begins with two underscores. Please search for it in the TI ARM compiler manual.
Thanks and regards,
-George
That's what I get for getting the answer from other questions on the forum as opposed to my source code!