This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/MSP-EXP430F5529LP: stuck compliling rts430x_lc_rd_eabi_se.lib

Part Number: MSP-EXP430F5529LP

Tool/software: TI C/C++ Compiler

building prevasivedisplays eink sample project for CCS

I encounter this message at build time:

warning #10366-D: automatic library build: using library "D:\ti\ccs1010\ccs\tools\compiler\ti-cgt-msp430_20.2.2.LTS\lib\rts430x_lc_rd_eabi_se.lib" for the first time, so it must be built.  This may take a few minutes.

I have aborted after 30+ minutes

ccstuio.exe and child processes lappear idle.

I periodically see ti- Code Composer Studio and Console Window Host jump to 0.1% CPU utilization.  Other than that, child processes are idle.

~100GB free on C drive and >200 GB free on D.  Drives are solid state.