Part Number: PROCESSOR-SDK-AM335X
Tool/software: Code Composer Studio
This is a CCS 10 I updated a while ago from CCCS 7.2...
Simply put... The project DOES NOT HAVE ANY ERRORS...
And yet the "problems" Window tells me there are 12. And these 12 errors the project NEVER had. Not in the past several YEARS. How did CCS 10 invent these??
No matter how many times I right click on it and clear it, it comes back in a few seconds and tells me there are 12.
No matter how many times I rebuild the entire project (no small task), it comes back in a few seconds and tells me there are 12.
These are NOT errors. I can pick one, and it goes to the "undefined" function... Then press F3 and it goes to the definition! Then obviously it can be resolved, and was!
How do you make CCS 10 stop LYING to me about errors?? It's kind of an important thing that I know where REAL errors are when compiling a project. Not phony ones.