Tool/software: Code Composer Studio
CCS version info:
Code Composer Studio
Version: 10.2.0.00009
OS: Windows 10, v.10.0, x86_64 / win32
Java version: 1.8.0_144
I am working with Tiva TM4c123 64pin part on custom board. I've been working with the FatFS code trying to port it to a WinBond spi serial flash.
I set a breakpoint (see below) at a line in a file. I then toggled the breakpoint to remove it, and it acts like the breakpoint is still active.
I have closed CCS v10 and re-opened, same problem. I have cleaned the project and rebuilt it, same problem (code halts at the line as if there is a breakpoint.
The menu item Run -> Remove all breakpoints is grey (indicating to me the user, that there are no breakpoints). When the program is loaded for debug, it stops at main() with a 'hidden' breakpoint at main().
Could it be that I somehow inadvertantly added a hidden breakpoint on line shown below. If so, is there a way to remove the hidden breakpoint?
What else could explain this behavior?
Thanks in advance