How do I easily find where a header file is stored. Or how do I find which "includes" location do I need to add for a specific header file.
If I open an MSP432 Simplelink example then I select the header file name and right click I can select "Open Declaration" and a copy of the header file will open. However, how can I find where this file came from or what folder location it is stored in?