This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Greetings...
This is the problem I encountered when trying to install MSP Compiler 19.6 with my existing CCS9.1.
FYI...I already have two other TI MSP430 Compiler 18 and 20, I wonder if this is the cause of this problem?
I need install this version of compiler since the imported project is dependent on it.
Thank you for your help!
Min
Hello Min,
Were you able to get the compiler installed? It looks like it's complaining about Sys-Config, which is a tool mostly used for figuring out pin-outs and generating some configuration code for some of our SimpleLink products. I'm guessing sys-config was updated with compiler 20, and now maybe trying to revert to an old version and is somehow conflicting...
Maybe you can install a new instance of code composer in a new folder, and install the required compiler there? You would have to open different instances for the different compilers, but I think it should work.
Let me know.
Thanks,
JD