Good morning,
I am currently an undergraduate student at the Democritus University of Thrace in Greece performing my dissertation thesis in the field of biomedicine. For this purpose, my colleagues and I, would like to develop a system of wearable sensors that will enable the continuous monitoring of vital biomedical parameters such as the body temperature, the blood pressure, the saturation of oxygen in blood, the hearth rhythm, as well as the electrocardiogram.
Through my navigation to your site and having previously looked into various scientific papers, I did not manage to find exactly the appropriate equipment that I will need to fulfil my thesis. However, as I was looking into your site and your previous project , I noticed that the TIIDA-01580 (Wireless ECG, SpO2, PTT and heart rate monitor reference design for medical and consumer wearables) is very close to the project I have undertaken in order to consider it as a model. However, as I mentioned above in the system that I want to design that will have the shape of a bracelet, I will want to monitor and take measurements for blood pressure and blood glucose monitoring. So, do you know if this happens ??
If so, how can I include the monitoring of these biomedical parameters in my system that I want to design and which parts are compatible and suitable ??
Kind Regards,
Sotiris Katsimentes