Other Parts Discussed in Thread: LMR50410, LM393LV, OPA2376
Dear Expert
I would like to make a simulation of LMR50410Y3F-Q1 step-down converter. There is no simulation model in Tina or Webench Power Designer so I have to use Pspice for TI. I download simulation model from https://www.ti.com/lit/zip/slum770 and I opened the simulation file.
I change some parameters and I saw the note that " The simulation runs for 2.4ms and takes approximately 60 minutes to run on a 4 core 2.8GHz machine." I didn't want to believe and I checked simulation parameters. Max step size was set 8ns and I made it 400ns (I removed also and left blank) and I set 2.6ms simulation and it took about 40 minutes. I realized and I made a mistake and I changed one parameter and I started the simulation again and it took another 40 minutes. It is unbelievable. I cannot make the simulation duration short because the IC cannot start to produce output before 1.8ms due to soft-start up feature.
How can I make the simulation faster? I use LTspice and I made similar simulation using LT3502 (it works at 2.2MHz as like LMR50410) and the simulation takes 30 seconds (2.6ms simulation duration).
There is a speed option in the simulation setting window and the default value is 3 and I left it 3. I think the software is so slow or so complex. It may give very very very accurate result but it is so slow and become useless. Who can wait 60 minutes for 2.4ms simulation? I think that if there is a way to make it faster TI didn't write a note that 2.4ms simulation takes 60 minutes.
Shall I change Gmin value or what I can do to make it faster as like Ltspice?
Best Regards