Other Parts Discussed in Thread: TIDA-01552, , LM5069, INA186
Hi Team,
Can you please check and advise with following request?
"
We are planning to make a fuse similar to eFuse (tidu415) in the vehicles we manufacture. In general, we plan this module to basically do the following operations. Apart from these, we will do features such as CAN BUS, analog voltage reading, warnings with microcontrollers. Do you have an integrated module that can do the below features?
- It can output 28V, 50A
- Short-circuit control, in this case, it turns off the output for a certain period of time and then gives the output again.
- Output current drawn as analog value
- Able to turn on/off output when requested
- Reverse battery protection
- “softstart” feature to prevent “inrush current”
"
Thanks in advance
Best Regards
Furkan Sefiloglu