I use TI UniFlash in a corporate network behind a proxy server to flash C2000 micro controller. In all UniFlash versions I've used, there is a bug that prevents this.
After pressing the "Load image" button, the error "Cannot read property 'DS' of undefined" occurs after a few seconds and the process is aborted. However, there is an annoying workaround. After all network connections have been switched off, the utility works as expected.
But this behaviour has now changed. With version 7 of UniFlash the error "Cannot read property 'DS' of undefined" always occurs, regardless of the state of the computer's network connection :-(
Is there any other tool available to flash TI micro controller via JTAG? Or may I hope that TI will try to fix this issue in the near future?