This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can some one share clear documentation for starting the TIDA 010042. I flashed the program using ez-Fet lite. Now i want clear documention or suitable material to start the board for experiments. I want to use Electronic load instead of batteries. Kindly help me.
Hello,
Thanks for your question. For connecting an electronic load, actually we have an answer from the other thread:
Pls let me know if you have any further question.
Regards
Lei
Hi Team,
ITs nt working in that way.
1) If pwm pulses are generating or not?
2) is there any other procedure to check board is working or not?
3) is there any possibility to check in code whether code works or not?
kinly guide me.
thanks
Hi,
This is easy to check.
1) make sure the SW is programmed to the MSP430 and able to run it via CCS
2) simply apply 24V on the DC input(panel in), and measure the output voltage at battery terminals, even with the open loop you should be able to measure a voltage ~12V
3) if you get a voltage at step 2), then you can probe the PWM signals on board
Regards
Lei
Hi sir, I checked the IC and the pulse provided to the MOSFET pulses coming out of IC but the board is not working.
kindy suggest me some solution
Hi,
can you pls describe your setup?
Btw, do you have any support from our local FAE team? Remote debug is a little bit challenging.
Regards
Lei
Hi sir,
I deeloped the board from design files from TIDA 010042 and used the firmware provided alog with that.
in the program i set the code for 12v system and run in the ccs.
and build it using the same (i referend some videos on ccs but not exctly dono whether coded succesfully or not)
I dont get any support as of now. but if possible can you connect with team viewer or any desk?