I have one workstation, two active windows installs. I'm guessing it is counting previous windows installation as I hop between stable, beta, and dev branches of windows every 6 months or so.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have one workstation, two active windows installs. I'm guessing it is counting previous windows installation as I hop between stable, beta, and dev branches of windows every 6 months or so.
Austin,
I don't think a new HD would have mattered. I can send you the names of the 3 machines we disabled.
-JC
I didn't just add a new drive, I installed windows to the new drive. I don't know the specifics of PSpice's host id creation, but serial number of boot drive is a pretty common piece. I saw the 3 names you sent in an email notification. First change was from a 6700k to a 5900x CPU and second change was from a 960 evo boot drive to a WD sn750. With the exception of the most recent one, those installations have long been overwritten.
OK, sounds like enough to warrant a host identification change.
Happy simulating!