This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
PSPICE-FOR-TI was crashed when I clicked "Edit Simulation Profile/ Run simulation".
Hi Akhil,
Please follow this FAQ to share the project with us. Also, do you remember what were you doing before this happened?
Thanks,
JC
When I changed the compressed file from .7z to .zip, I could able to upload error log file. Please check the attached error log.
Yes. The first step is to try open or create another project to see if you have the same problem. If you have trouble with every project you have created, there's something for you to try:
1. Close PSpice and other Cadence tools which are running.
2. Open Task Manager and make sure that none of the below processes are running. If they are running, end them manually.
a. MrKSrvr.exe
b. PSpiceExplorerSrvr.exe
c. Simmgr.exe
d. SimSrvr.exe
e. Pspice.exe
f. Capture.exe
3. Now restart the machine and rename folder OrCAD_CaptureTIPSpice_Install present at <%CDS_HOME%>\cdssetup to OrCAD_CaptureTIPSpice_Install_OLD and OrCAD_PSpiceTIPSpice_Install to OrCAD_PSpiceTIPSpice_Install_OLD.
4. Now, in start menu type regedit and click on registry editor to open it. Go to HKEY_CURRENT_USER\Software\Orcad\ and delete the CaptureTIPSpice_Install folder.
5. Open the project you had problem with and try running a simulation to see if the issue goes away.
Thanks!
-JC
Hi JC,
Yes, I had trouble with every project that I had created, so I followed the steps you suggested and now the issue has been resolved.
Thank you very much for your support!