Other Parts Discussed in Thread: LM5155, LM5175, LM5176
Hi,
I was simulated LM5122 circuit in PSpice for TI earlier.I plan to use the LM5122 circuit to control the boost. In the datasheet of that circuit, there is a proposal where it is controlled using a voltage divider from the output that is fed to the FB pin.
However, I need to operate the steering by electricity. I need to filter the current signal from the saw-shaped shunt (maximum 30 mV voltage) and amplify it 10 times (this would be done by the first part of the circuit),
and then give the second part of the circuit, on which the value is set, the current value (shown also by the voltage, which will after amplification the maximum will be 300 mV),
regulate according to the mean value of the current and that the voltage at the output of 1.2 V is fed to the FB pin of the circuit LM5122 (internal error amplifier) which will start the circuit to do the regulation.
In short, can you offer a circuit that will do regulation by the mean value of the choke current? I need to modify the LM5122 circuit, by removing the voltage control offered in your datasheet,
and adding a current control that represents a feedback loop that leads from the shunt to the FB pin of the circuit.
Best regards,
Đorđe