Other Parts Discussed in Thread: LMR23615
I have an issue with the brand new installation of PSpice for TI. I just stated the first tutorial in 'Labs.pdf' and tried to get the bias point, but see the error that seemed to be solved 2 years ago, but the steps are not applicable because the menu items mentioned in the solution are not there. This is the error message:
** Creating circuit file "bias.cir"
** WARNING: THIS AUTOMATICALLY GENERATED FILE MAY BE OVERWRITTEN BY SUBSEQUENT SIMULATIONS
*Libraries:
* Profile Libraries :
* Local Libraries :
* From [PSPICE NETLIST] section of C:\cds_spb_home\cdssetup\OrCAD_PSpiceTIPSpice_Install\17.4.0\PSpice.ini file:
.lib "nom_pspti.lib"
.lib "nom.lib"
*Analysis directives:
.OP
.OPTIONS ADVCONV
.OPTIONS FILEMODELSEARCH
.PROBE64 V(alias(*)) I(alias(*)) W(alias(*)) D(alias(*)) NOISE(alias(*))
.INC "..\SCHEMATIC1.net"
**** INCLUDING SCHEMATIC1.net ****
* source RC
V_V1 IN N14409 10V
R_R1 OUT IN 1k TC=0,0
R_R2 OUT N14409 1k TC=0,0
C_Cap1 OUT N14409 1n TC=0,0
**** RESUMING bias.cir ****
.END
WARNING(ORPSIM-15246): Library index file nom_pspti.ind does not have the correct format
INFO(ORPSIM-15422): Making new index file nom_pspti.ind for library file nom_pspti.lib.
.lib "LMR23615_TRANS.LIB"
ERROR(ORPSIM-15116): Unable to find library file LMR23615_TRANS.LIB.
Index has 12646 entries from 801 file(s).
ERROR(ORPSIM-15107): Unable to make index for library file C:\cds_spb_home\cdssetup\pspTILibDir\nom_pspti.lib.
Please help! Thanks