Part Number: PMP41006
Hello,
I am looking for the specifications of L6 and L4 used in this design(details / datasheets / cores used)
Unable to find anything in the resource files, kindly provide me with the same?
Regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PMP41006
Hello,
I am looking for the specifications of L6 and L4 used in this design(details / datasheets / cores used)
Unable to find anything in the resource files, kindly provide me with the same?
Regards,
1000W PFC Choke L=300uH Rev A -SPEC.pdf1000W Common Mode Choke-YXS80466T-Rev A -SPEC.pdf
Hi
I put their datasheet in above attachments.
While, just let you know, I recently found the L4 may introduce oscillation to the input current. So it maybe removed later.
Hello Desheng,
Thanks for providing the datasheet and warning about the oscillations due to L4, will keep that in mind.
I have a few queries related to the datasheet.
- The first three cores looks like options/substitutes of each other. Is that correct?
- Why are the two Alloy cores listed here, are these options for above ferrite cores?
Regards,
Yes I think they are substitutes.
The alloy core is added to the ferrite core, the two parts should same are substitutes to each other.