Part Number: TIDA-00289
Other Parts Discussed in Thread: DRV110
During the Design about the Solenoid Controll system.
I detect the solenoid movement about current characteristics of solenoid.
I want to make solenoid current to 0A when EN signal is Low. And the Gate Signal from DRV110(OUT) is Low.
According to figure 43. Test result, Solenoid Current still was maintain according to I hold level.
So, When i make current value to 0A, i change the R hold resister?! or just R hold resister will be stable to 0 ohms condition.
best regard.