Hi' Another question I have is this. When I examined the Filter bode plot in the reference design, it was written that it guarantees 0.7Hz. When I analyzed the Bode plot graph with an opamp these capacitor and resistor values , it was seen that it attenuated the signal by -2.4973dB at 0.7Hz. Don't we want the gain to be 0dB at 0.7Hz? (-2.4973dB) isn't fold reduction a bad value for iepe sensor input in low frequnecies like 0.7 ?
Do you have any other suggestions to improve this? Increasing the filter order etc.