I have the same error: After starting the installation the following message appears:
"An Internal error occured. Please go to http://e2e.ti.com for further assistance. (-1)

Is there a simple solution to resolve this ?
Thanks Manfred
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have the same error: After starting the installation the following message appears:
"An Internal error occured. Please go to http://e2e.ti.com for further assistance. (-1)

Is there a simple solution to resolve this ?
Thanks Manfred
Hi Manfred,
We've recevied a lot of reports of this problem and it is being actively worked on. I'll let you know when we have a fix.
David
Thanks Manfred. I've got another that's done the same and have referred that to Cadence. I'll also push these to IT in case there's something else going on.
David
Hi Manfred,
Please try replacing your config file with the following file.
Location: %AppData%
<?xml version="1.0" encoding="utf-8" ?>
<configuration>
<startup>
<supportedRuntime version="v4.0" sku=".NETFramework,Version=v4.5"/>
<supportedRuntime version="v4.0"/>
<supportedRuntime version="v2.0.50727"/>
</startup>
</configuration>
David
The magic of a new year, I guess.
Not sure what happened as this impacted a number of people and then seemed to self-resolve.
Would be nice to know a corrective action so that we could attack this quicker. Sorry for the invconvenience.
Regards,
David