Part Number: TIDA-01606
Other Parts Discussed in Thread: TMDSCNCD28379D, TMDSHSECDOCK, UNIFLASH, TMS320F28379D
Dear TI,
I have uploaded this question, but the answer does not help to solve the issue.
Thus, I upload this problem again and I will explain more in detail.
I got the error like the below message.
I think my computer can not access device register.
I am using F28379D(TMDSCNCD28379D) and I did what the manual said in 3.1.1.3 F28377D, F28379D Control-Card Settings.
And the board was populated the power circuit and MCU connector.
When I put the MCU on the main board, it shows the proper light which means the board has the proper power.
Also, I tested the MCU on the TMDSHSECDOCK.
And it is working properly.
Could you give me a guild to solve this issue?
Error in build step #3 (Make): Make process exited with code 2:
copy /Y "F:\1. 2023\5. PLECS\tsp_ti_c2000\templates\uniflash\ControlCard_TMS320F28379D.ccxml" ".\output_TI2837xS_cpu1\MSU.ccxml"
1 Ǿ ϴ .
"C:/ti/uniflash_8.2.0/dslite.bat" --flash --config=.\output_TI2837xS_cpu1\MSU.ccxml .\output_TI2837xS_cpu1\MSU.out -u
Executing the following command:
> "C:\ti\uniflash_8.2.0\deskdb\content\TICloudAgent\win\ccs_base\DebugServer\bin\DSLite" flash --flash --config=.\output_TI2837xS_cpu1\MSU.ccxml .\output_TI2837xS_cpu1\MSU.out -u
For more details and examples, please refer to the UniFlash Quick Start guide.
fatal: IcePick_C_0: Error connecting to the target: (Error -2131 @ 0x0) Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.10.0.00080)
MSU.mk:157: recipe for target 'download' failed
Failed: Operation was aborted
make: *** [download] Error 1