Other Parts Discussed in Thread: PMP10195, , PMP12082, PMP41063, PMP41031, PMP10415
Hi,
We need to develop the isolated DC-DC converter. You can see the specifications below. In addition, we need additional at least 5000kV isolation rating between primary and secondary. Are there any alternative solutions to PMP30495 and PMP12082 that you could recommend for meeting these specifications? The PMP10195 or PMP41063 schematic is also good option, could you please suggest 12V output alternative of that reference, if possible?
Best regards
| Design Values | ||
| Min Input Voltage | 360 | V |
| Max Input Voltage | 630 | V |
| Output Voltage | 12 | V |
| Output Current | 1 | A |