This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP30495: 3-phase Input to 12VDC converter

Part Number: PMP30495


Tool/software:

Hi,

I want to convert 3-phase AC line voltage with each phase voltage range of 85VAC-250VAC and convert it into 12VDC 1.5A output. The supply should be able to provide the required output even if only one phase is available and the other two phases are down. I came accross this reference design PMP30495. Will this be able to provide output even if any one phase is available? Why R16 here is for test purpose I mean if R16 is DNP then this whole section will be of no use? Any recommeded part number of transformer for single 12V output that is available easily.