This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, I found this design:
35V to 60V Input, 600W Output Dual-Phase Buck Converter Design with Greater than 97% Efficiency
http://www.ti.com/tool/PMP7282#technicaldocuments (2012)
What newer products are there that will help achieving high efficiency and power output at 12V with a wide DC input range.
its possible I can nail down an input range but from my understanding the PWM technique should allow a wide range with minimal losses, unless I'm missing something?
Hi Katelyn,
Thanks for following up!
If there are certain requirements to gain >97%+ efficiency, we can tailor the input to that range, but I'd like to be as adaptable as possible.
Right now for our project, the input range can vary between 30VDC -1000VDC. In actuality it will be anywhere in that range +/- 10VDC. It comes down to wiring losses which become meaningful based on the distance from the power source to where its being used.
ex: one system may have an input at 70VDC +/- 10VDC ( 60VDC - 80VDC)
another system may have 380VDC +/- 10VDC (370VDC - 390VDC)
Does that make sense?
The other thing about the PMP7282 design is it puts out a lot of heat! It gets over 100 C at 50A load based on the test data. I was hoping new devices could help get into a more manageable range (~50 C) or if we could parallelize the boards (PMP7282 reaches peak efficiency @ 30 A) to achieve the same while maintaining modularity.
Kind regards,
sug
Hello,
One option may be the LM5140-Q1 65V synchronous dual controller that can be configured as a two-phase implementation. The LM5146-Q1 may also be a possibility. Note that the 12V output can feed the VCC of the LM5146-Q1 to reduce IC power consumption. See this blog to configure as a two-phase implementation:
What is the output current requirement? Maybe an efficient single-phase implementation is feasible.
Regards,
Tim
Hi Tim,
Thanks for the link, it was helpful.
I overlooked the potential phase shift from parallelized DC-DC converters. I figured a system that took multiple DC 12V outputs and then fed into a regulator would suffice but this is a potential for efficiency gains or losses depending on how its handled.
Each system/unit will require 550W - 600W. [edit: we may be able to optimize each system to ~450W but I'd like to allow for a margin]
Some devices will use far less, ~150W. They can be handled with conventional products or bundled to reach similar power usage.
Kind regards,
sug