Other Parts Discussed in Thread: LM5157
Tool/software:
Hi,
Iam Doing the Sepic Converter Simulation using the LM5157 IC Model, Transient analysis is taking normally 20 to 30 minutes for 3mS duration simulation. But, when i am doing the DC Sweep simulation its taking almost more than 20 hours time, how to reduce the time for DC Sweep simulation, and after completing the simulation its not providing any result.
I am sweeping the input voltage from 8.5V to 22V with 1V increment,
After that I have changed the simulation settings as below, and the simulation time is reduced to 30 minutes, but not output is observed. Its showing the error like There are no data values in section number 1, ignoring this section, Next error Analysis failed.
Reduced ITL4 to 5
Changed PTRANABSTOL: 1e^-5
Changed PTRANVNTOL: 1e^-4
My Simulation settings are shown below,
is there any other Methode to reduce this timing and do the DC Sweep analysis?
Regards
Rayees K.E