Part Number: PMP22650
Tool/software:
Hello,
I have a doubt about the selection of the bus electrolytic capacitors.
From the BOM, the capacitors selected are the ALA7DA471DE500 from Kemet. 470uF, 500V and 2.5A@100Hz ripple current.
3 caps in parallel therefore 7.5 A, I’ve estimate and simulate the current ripple across the line cycle, and I have obtained a rms current of 17A.
How it is possible that this cap can handle all the current?
Thanks in advance.