Part Number: UCC3895
Other Parts Discussed in Thread: UCC2895, UCC28950
Tool/software:
UCC3895/UCC2895 : Phase Shift Full Bridge
Hello,
I'm using the UCC3895 for a PSFB with high voltage ratio x30.
The frequency is arround 20kHz for the application. I've done the simulation with
PSpice for TI and it works well. However, in the datasheet, the minimum frequency of the IC is 50kHz.
Is it physically problematic if I use it at 20kHz.
In advance, many thanks for your return.