This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello experts
Hope this finds you well.
My customer want to buy and use evaluation board to verify the operation.
For the configuration, refer to your Battery energy storage system page
Battery management IC: BQ79616
Bridge IC: BQ79600
MCU: AM263P4
SO
They are considering purchasing BQ79616EVM-021, BQ79600EVM and LP-AM263P respectively.
We would like to ask you to review:
. If we want to implement the above configurations with the purchase of each evaluation board,
Are there any other accessories required for each connection?
Between AM263P4 and battery IC.
Regards,
Jieyu Zhou
Jieyu,
I have looped our designer of TIDA-010271 to help here, please expect another day for the reply.
Ryan
Jieyu,
Several wires is needed from BQ79600 EVM to MCU board. It is 5 dupont wires if SPI is used.
In stead of LP-AM263P, I suggest TMDSCNCD263P and TMDSHSECDOCK, which i have tested it before. If LP-AM263P is used, it should be necessary to check if 1 SPI and GPIO interface is available.