Part Number: AFE58JD48EVM
Other Parts Discussed in Thread: TSW14J50EVM, , AFE58JD48
Tool/software:
Hello
I have a TSW14J50EVM connected to an AFE58JD48EVM.
I can sample waveforms from HDSC Pro (version 5.20) properly but the trigger options do not work.
The trigger options are configured as follows:

I feed a 3.3V 100ns wide trigger pulse to TRIG_IN SMA connector but the capture does no start. HDSC shows “TRIGGERED ARMED” continuously but does not respond to my trigger.


After I select “trigger mode enable” and “arm on next capture button press”, and click generate “generate trigger”, HSDC waits a while and shows “no trigger occurred”.

I tried the following configurations, but they all failed :
User profile AFE58JD48_Custom_PLL_MODE_40x_No Demod_SubClass1 、
Firmware AFE58JD48.ini
Please tell me what needs to be done to make the external trigger work